usb driver for windows10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

usb driver for windows10

1,978 次查看
1029124854
Contributor I

LPC2148 usb  driver for windows10.

0 项奖励
回复
1 回复

1,753 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Jackie,

The LPC21xx is part of the legacy devices and it has limited support. If you are referring to the USB drivers related to the debugger, you could contact to board manufacturer to ask of there is an updated version. Otherwise, you may consider using an external debugger with updated drivers, like Segger J-Link.

If you refer to custom USB drivers from a programmed USB application on the MCU, I’m afraid that we don’t have, although some of the generic USB drivers (like HID, MSD, CDC) are usually included on the newer operating system, just requiring some modification on the USB descriptors.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复