usb communication in lpc55S16 JBD100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usb communication in lpc55S16 JBD100

5,043 Views
Arularasan
Contributor II

i have done all the procedure in lpc55S16 JBD100 with the help MCUXpresso IDE.

example code generated MCUXpresso IDE. read and write function is not created, kindly help me the steps to read and write in pendriver through USB communication in lpc55S16 JBD100 iam using USB1 HOST.

0 Kudos
Reply
7 Replies

5,003 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Arularasan 

There is USB HOST demo under SDK, you can refer to, download from:

https://mcuxpresso.nxp.com/en/select  

Alice_Yang_0-1677466883455.png

 

BR

Alice

 

0 Kudos
Reply

4,998 Views
Arularasan
Contributor II

@Alice_Yang thanks for your reply.

USB HOST demo under SDK example code ("host_msd_fatfs_bm") I have download  but its not working !

I want to read and write in pen drive through usb communication iam using USB1. 

kindly help me @Alice_Yang 

0 Kudos
Reply

4,978 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Arularasan 

 

"but its not working"

->>  Please tell me the details of the "not working"  and how do you run it. My colleague have tested this demo, it can work well.

 

BR

Alice

0 Kudos
Reply

4,965 Views
Arularasan
Contributor II

thanks for your reply @Alice_Yang 

in debug mode 

it prints only " host init done "

when I plug in u disk in USB1 nothing is printed in terminal.

please reply @Alice_Yang 

0 Kudos
Reply

4,906 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Arularasan 

The default USB of this demo is USB0, if you want to use USB1, you need change some code, and jumper on board.

Change code as below:

.2   Update USB host demo: USB0->USB1

Taking usb_host_hid_mouse demo code as an example, to switch to USB1, modify the macro definition in usb_host_config.h as follows:

#defineUSB_HOST_CONFIG_KHCI (0U)

#defineUSB_HOST_CONFIG_EHCI (0U)

#define USB_HOST_CONFIG_OHCI (0U)

#define USB_HOST_CONFIG_IP3516HS (1U)

Jumpers refer to readme.txt, I also tested on my side, works well, jumpers as below:

Alice_Yang_0-1678176451077.png

 

 

BR

Alice

 

0 Kudos
Reply

4,875 Views
Arularasan
Contributor II

@Alice_Yang thanks for your support 

After modify demo code  lpcxpresso55s16_host_msd_fatfs_bm    macro definition in usb_host_config.h and jumpers to USB1   It detects the mass storage device

kindly help me to write and read in mass storage device(PEN DRIVE)

in debug session

(

host init done
mass storage device attached:pid=0x558avid=0x781 address=1
............................fatfs test.....................
fatfs mount as logiacal driver 1......success
test f_mkfs......success
test f_getfree:
FAT type = FAT32
bytes per cluster = 32768; number of clusters=938764
The free size: 30040416KB, the total size:30040448KB
directory operation:
list root directory:

create directory "dir_1"......success
create directory "dir_2"......success
create sub directory "dir_2/sub_1"......success
list root directory:
dir - ___ - DIR_1 - 0Bytes - 2018-1-1 0:0:0
dir - ___ - DIR_2 - 0Bytes - 2018-1-1 0:0:0
list directory "dir_1":
dir - ___ - SUB_1 - 0Bytes - 2018-1-1 0:0:0
rename directory "dir_1/sub_1" to "dir_1/sub_2"......success
delete directory "dir_1/sub_2"......success
get directory "dir_1" information:
dir - ___ - DIR_1 - 0Bytes - 2018-1-1 0:0:0
change "dir_1" timestamp to 2015.10.1, 12:30:0......success
get directory "dir_1" information:
dir - ___ - DIR_1 - 0Bytes - 2015-10-1 12:30:0
file operation:
create file "f_1.dat"......success
test f_write......success
test f_printf......success
test f_puts......success
test f_putc......success
test f_seek......success
test f_gets......ABCDEFGHI
test f_read......JKLMNOPQRS
test f_truncate......success
test f_close......success
get file "f_1.dat" information:
fil - ___ - F_1.DAT - 19Bytes - 2018-1-1 0:0:0
change "f_1.dat" timestamp to 2015.10.1, 12:30:0......success
change "f_1.dat" to readonly......success
get file "f_1.dat" information:
fil - R__ - F_1.DAT - 19Bytes - 2015-10-1 12:30:0
remove "f_1.dat" readonly attribute......success
get file "f_1.dat" information:
fil - ___ - F_1.DAT - 19Bytes - 2015-10-1 12:30:0
rename "f_1.dat" to "f_2.dat"......success
delete "f_2.dat"......success
............................test done......................

)

 

 

0 Kudos
Reply

4,846 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Arularasan 

 

You can refer to readme.pdf, config "throughput test", there is write and read function code.

 

BR

Alice

0 Kudos
Reply