usb bulk问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usb bulk问题

2,515 Views
万朋朋pengpeng
Contributor I

LPC54606的高速usb实现自定义设备,bulk传输已经实现,但是有问题

我的实现思路是:设立端点空闲标志,发送请求成功后,标志位设置为发送中,回调函数中设置为发送完成。但是有时会出现发送请求成功,但是端点回调函数没有被调用的问题,导致标志位不能被改变,所以不能继续发送。为保证数据发送完成同时提高速率,有什么好的建议吗?

Labels (3)
0 Kudos
Reply
1 Reply

2,293 Views
jeremyzhou
NXP Employee
NXP Employee

Hi 万朋朋 pengpeng,

非常感谢使用NXP产品,很高兴为你提供技术支持!
请问你是基于SDK中USB stack实现USB应用的吗?
还有你的工程基于MSC工程为模板修改的呢还是从零开始创建的,最好你可以介绍一下你的工程的实现过程,方便问题查找。


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply