usb bootloader extension ??

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

usb bootloader extension ??

1,231件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leonardo on Fri Jan 11 00:10:21 MST 2013
Hi

    I looking for an extension to the AN10866 usb boot loader application note from NXP .
I wish apart from standard functionality to have a second file located in external spi flash .
So after connection to my LPC1752 module PC sees two files one with size up to 128K located
in flash and the second up to 4 MB located in spi flash .As I understand wwe need a second entry to the
fat and a redirection of the IAP programming to work with flash pages over the 128K .
Has anybody done that ?.Can anybody assist me ?




ラベル(1)
  • USB

0 件の賞賛
返信
0 返答(返信)