usb bootloader extension ??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usb bootloader extension ??

1,226 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leonardo on Fri Jan 11 00:10:21 MST 2013
Hi

    I looking for an extension to the AN10866 usb boot loader application note from NXP .
I wish apart from standard functionality to have a second file located in external spi flash .
So after connection to my LPC1752 module PC sees two files one with size up to 128K located
in flash and the second up to 4 MB located in spi flash .As I understand wwe need a second entry to the
fat and a redirection of the IAP programming to work with flash pages over the 128K .
Has anybody done that ?.Can anybody assist me ?




Labels (1)
0 Kudos
Reply
0 Replies