usb bootloader LPC1343

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usb bootloader LPC1343

4,406 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by grutjespap on Wed Jul 17 04:22:53 MST 2013
Hi, i can't seem to get the usb isp bootloader thingy to work, windows reports unreconized device, and osx/linux does nothing.

http://embeddedartists.com/support/qsb/lpc1343 is the board that i have.

Does anybody have a idea? (also i haved got any of the usb example running)


Labels (1)
0 Kudos
Reply
3 Replies

4,137 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Wed Sep 18 06:06:27 MST 2013
Try pressing the BL (bootloader) button on the EA LPC1343 board while plugging the device into a USB port.  It should enter ISP mode, and assuming that VBUS is high, it should show up as a mass storage device on your PC.
If that doesn't work, with the hardware already plugged into the PC, try pressing the BL button, then press and release the RESET button.  The LPC1343 should show up as a mass storage device on your PC.

- Paul
0 Kudos
Reply

4,137 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by grutjespap on Tue Sep 10 12:20:05 MST 2013

Quote: pdpro
Does your connected device get detected in Windows as CRP DISABLED ?? then follow these steps....
Use NXPISP utility program from documentation section of NXP site for LPC1343. This utility will update your IC in CRP DISABLED mode with a simple valid blink program. It will look like this image I've attached....

    If not detected then check whether device manager shows it as Human Interface Device(HID). If so then the firmware is already updated with some program.


It does not show on Windows or mac or linux.
0 Kudos
Reply

4,137 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pdpro on Sat Aug 31 06:09:31 MST 2013
    Does your connected device get detected in Windows as CRP DISABLED ?? then follow these steps....
Use NXPISP utility program from documentation section of NXP site for LPC1343. This utility will update your IC in CRP DISABLED mode with a simple valid blink program. It will look like this image I've attached....

    If not detected then check whether device manager shows it as Human Interface Device(HID). If so then the firmware is already updated with some program.
0 Kudos
Reply