uestions about Emcraft Systems Linux for LPC1788

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uestions about Emcraft Systems Linux for LPC1788

1,229件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by thomas.jing on Thu Aug 16 22:12:29 MST 2012
> bootm a0008000
## Booting kernel from Legacy Image at a0008000 ...
   Image Name:   Linux-2.6.33-arm1
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2131712 Bytes =  2 MB
   Load Address: a0008000
   Entry Point:  a0008001
   Verifying Checksum ... OK
   XIP Kernel Image ... OK
OK

Starting kernel ...

it's halting here .
I only changed the lpc178x_iomux_init(function );just changed the ea_lpc1788_gpio[] = {};
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,215件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by thomas.jing on Fri Aug 17 01:08:25 MST 2012
Sorry it's my fault,the issue has settled.
0 件の賞賛
返信

1,215件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by thomas.jing on Thu Aug 16 23:57:24 MST 2012
If i not changed the lpc178x_iomux_init(function )(just changed the ea_lpc1788_gpio[] = {};) use the original Emcraft Systems Linux for LPC1788 1.4  the kernel running well.
who can help me?
0 件の賞賛
返信