uart receiver problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

uart receiver problem

跳至解决方案
1,248 次查看
Berlin
Contributor I

I'm using the LPC865M201JHI48 microcontroller for UART communication. The transmit function works correctly using polling method  (I verified this using a serial terminal like PuTTY), but the receive function is not working properly. if there any example code?

标签 (1)
0 项奖励
回复
1 解答
1,237 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @Berlin 

You can refer to the lpc860 SDK UART demo code.

Select Board | MCUXpresso SDK Builder

Harry_Zhang_0-1751885423735.png

BR

Harry

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,238 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @Berlin 

You can refer to the lpc860 SDK UART demo code.

Select Board | MCUXpresso SDK Builder

Harry_Zhang_0-1751885423735.png

BR

Harry

 

0 项奖励
回复