uart receiver problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uart receiver problem

ソリューションへジャンプ
1,244件の閲覧回数
Berlin
Contributor I

I'm using the LPC865M201JHI48 microcontroller for UART communication. The transmit function works correctly using polling method  (I verified this using a serial terminal like PuTTY), but the receive function is not working properly. if there any example code?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,233件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @Berlin 

You can refer to the lpc860 SDK UART demo code.

Select Board | MCUXpresso SDK Builder

Harry_Zhang_0-1751885423735.png

BR

Harry

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,234件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @Berlin 

You can refer to the lpc860 SDK UART demo code.

Select Board | MCUXpresso SDK Builder

Harry_Zhang_0-1751885423735.png

BR

Harry

 

0 件の賞賛
返信