uTasker compiled in LPCXpresso_7.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uTasker compiled in LPCXpresso_7.3

1,063 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kiryat8 on Tue Aug 19 05:30:10 MST 2014
Shalom!
Is it possible to compile and debug an uTasker project in the LPCXpresso_7.3 IDE?
The uTasker project has several features that I would like to use in my project.

The uTasker project will build from a GCC make file so may able to work
with Code Red (I believe that Code Red is an Eclipse based environment
using GCC).

Has anyone tried?

I had posted this previously in the general forum by mistake.

Thanks
Labels (1)
0 Kudos
Reply
1 Reply

1,054 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Aug 20 02:26:32 MST 2014
Please don't create duplicate threads. I suggest you delete this thread.

Response posted at:

http://www.lpcware.com/content/forum/utasker-compiled-lpcxpresso73#comment-1139455

0 Kudos
Reply