uEZ GUI 1788-70WVT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uEZ GUI 1788-70WVT

2,000 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by halitkaya60 on Thu Aug 15 23:21:12 MST 2013
Hi,

I have uEZ GUI 1788-70wvt development kit. I am a student and any experience on this technology. I try to make a GUI application for this kit. Like add video, background picture, music, button and icons. There are many programs to develop the project. CrossWork Studio, Iar Embedded workbench, Keil uvision, Lpcxpresso and code red. I'm so confused which program should be used. And also for GUI desinged how can make easily programmed. Gui builder or other

Regard,
Halit
Labels (1)
0 Kudos
Reply
3 Replies

1,942 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by halitkaya60 on Tue Aug 20 00:53:46 MST 2013
Hi,

uEZ GUI 1788-70WVT manufactured by FDI. When I ask the their forum for programming they offer to use CrossWork studio, Iar embedded workbench and keil uvision. And also for video and music display, they said "uEZGUI-EXP-DK kit is using for this example. You purcgase this kit"

uEZ GUI 1788-70wvt has its own jlink lite Arm debugger. When I want to use lpcxpresso, this debugger doesn't support and I take a Lpc-link 2 and try to debug. I am download BSP file and load lpcxpresso succesfully. Lpcxpresso see the debugger but I see the computer screen "02: Failed to connect Ee(80) Hardware device not found". What can I do for these?

Rergards,
Halit
0 Kudos
Reply

1,942 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by halitkaya60 on Sun Aug 18 22:12:54 MST 2013
Hi,

Thanks for reply. I am look over these document.

Regards,
Halit
0 Kudos
Reply

1,942 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Fri Aug 16 11:03:52 MST 2013
Hi,
As you are a student, you can start using LPCXpresso,which is free upto 128KB. We have a dedicated page for emWin graphic here
http://lpcware.com/content/project/emwin-graphics-library

In this page, we have BSPs,emWin Libraries and documentation for your help. BSPs also contain a window based GUI builder, which you can use to generate C code for your application.
 
I recommend you to start with startup guide which is at

http://www.nxp.com/documents/application_note/AN11244.pdf

After this you can read porting guide which is at

http://www.lpcware.com/content/nxpfile/emwin-porting-guide-ea-lpc1788-bsp-keil-mcb1700-english-versi....

Hope it will help you to start your project.

-------
Thanks,
MC
0 Kudos
Reply