tfm_psatest_ns on LPCpresso55s69.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tfm_psatest_ns on LPCpresso55s69.

Jump to solution
1,924 Views
ShinjiOhishi
Contributor II

Hello.
I tried tfm_psatest_ns on LPCpresso55s69.
From "TEST: 226" to "TEST: 231" and "TEST: 234" are the same function is called.

lpcxpresso55s69_tfm_psatest_ns/api-tests/val/test_entry_list.inc

bug.pngbug.png

I think they are incorrect code.

If these are bugs, please fix them.

Thanks.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,901 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello ShinjiOhishi,

I edited my previous answer. I was confirmed that this is a typo and will be fixed on new releases of the SDK. Thank you for pointing this out!

Regards,
Gustavo

View solution in original post

0 Kudos
Reply
3 Replies
1,908 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello ShinjiOhishi,

Thank you for pointing this out.

It was confirmed that these are indeed typos. It was escalated to the SDK team know, and it will be fixed on future SDK releases.

My apologies for the inconvenience.

Regards,
Gustavo

0 Kudos
Reply
1,902 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello ShinjiOhishi,

I edited my previous answer. I was confirmed that this is a typo and will be fixed on new releases of the SDK. Thank you for pointing this out!

Regards,
Gustavo

0 Kudos
Reply
1,876 Views
ShinjiOhishi
Contributor II

Hello Gustavo.
Thank you for fixing it.

0 Kudos
Reply