.svd for LPC55S69?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

.svd for LPC55S69?

Jump to solution
2,791 Views
starblue
Contributor III

Is there a .svd file for LPC55S69 somewhere?

I would like to use it to generate Rust bindings.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,616 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Juefwn,

Please see LPC55S89.svd file attached.

Hope this helps.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

1 Reply
2,617 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Juefwn,

Please see LPC55S89.svd file attached.

Hope this helps.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------