startup LPC2468

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

startup LPC2468

3,718 Views
pieterbos
Contributor I

Hi, we have a design that worked for more than 7 years with the LPC2468 but lately we experience some problem with the startup. it only works when we touche the LSE crystal.

 

0 Kudos
Reply
11 Replies

3,689 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @pieterbos 

Based on your description, it strongly suggests a marginal oscillator startup issue—often caused by aging components, contamination, or environmental factors.

So i think you can try to Replace the Crystal and Check and Adjust Load Capacitors.

BR

Harry

0 Kudos
Reply

3,676 Views
pieterbos
Contributor I

Hi, 

We tried to do that but it didn't work

0 Kudos
Reply

3,594 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @pieterbos 

You can try  supplying an external 32.768 kHz signal (e.g. from a signal generator or test oscillator) to X1 to see if the system behaves correctly.

If the MCU starts reliably with this, the issue is almost certainly with the oscillator circuit.

If there is an issue with the oscillator circuit.

You can visual inspection under magnification for oxidation or corrosion around the crystal, capacitors, and oscillator pins (X1, X2).

Contaminants (e.g., flux residue) can create leakage paths or add parasitic capacitance.

BR

Harry

0 Kudos
Reply

3,456 Views
pieterbos
Contributor I

Hi Harry,

We tried but that did not solve the issue. 

With external clock it works but also only the calbe and not clock it will startup correctly. 

So it looks lijkt 1 pin needs a lot of capacitance / mass or somethine like that? 

0 Kudos
Reply

3,395 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @pieterbos 

Yes, 

Since touching or adding a cable helps:

Temporarily try adding small extra capacitance between OSC pins and GND ( e.g., 2pF, 4.7pF, 10pF).

Alternatively, add a high-value resistor across the crystal (some circuits benefit from this to kickstart oscillation).

BR

Harry

0 Kudos
Reply

3,359 Views
pieterbos
Contributor I

@Harry_Zhang 

Thank you for your reply,

We tried the following:

100k R || crystal. this did not work sadly. 

different C at only 1 leg and this did also not work....

 

 

0 Kudos
Reply

3,327 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @pieterbos 

Based on previous information, the issue is almost certainly with the oscillator circuit.

If GND near the crystal is noisy or not low-impedance, oscillation can be disturbed.

Try probing VRTC and GND with oscilloscope during startup to ensure no glitch.

BR

Harry

0 Kudos
Reply

3,324 Views
pieterbos
Contributor I

@Harry_Zhang 

I just probe the givin pin and the noise was at max 80uV

Is this in sec?

0 Kudos
Reply

3,288 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @pieterbos 

If you're seeing 80 µV on your probe when checking the RTC crystal pin.

You're only seeing noise, and the RTC crystal oscillator is not starting up. This confirms the issue is in the oscillator startup conditions, not external interference.

BR

Harry

0 Kudos
Reply

3,284 Views
pieterbos
Contributor I

@Harry_Zhang 

We found the problem, the PCBA maker did not was it properly and there was hidden flux and tin we could not see with the microscope. But after proper cleaning it works. Sorry for the trouble. 

0 Kudos
Reply

3,590 Views
pieterbos
Contributor I

Hi Harry,

We will try and come back with the resultes

0 Kudos
Reply