some information on the chip_18x_43xx folder

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

some information on the chip_18x_43xx folder

1,130 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pra18 on Tue Jul 29 03:45:43 MST 2014
Hi,

I need some information on the chip_18x_43xx folder in the lpcopen examples for ngx and hitex 4350 kits.

Are the sources inside these folder like clock_18xx_43xx.c/.h example implementation or to be used as it is ( NXP provided original sources)

For example , I want to port the code into my own custom lpc43xx board , can I use these functions directly or are they jsut examples.

In which case which functions do I need to really use , does there exist a source file equivalent like lpc_xxxx.c given by nxp to use ?
or do I need to provide my own  functions

Thanks in advance,
标签 (1)
0 项奖励
回复
1 回复

1,122 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Fri Aug 08 16:08:23 MST 2014
Hi, pra18,

Source files under chip_18x_43xx folder should be able to be ported to your own custom lpc43xx board.
They are however still sample programs, NXP does not assume any liability with the sample code.
Have a prefix of lpc_xxxx does not change the nature of the sample programs.

regards,
0 项奖励
回复