solid model LPC-Link 2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

solid model LPC-Link 2

1,733 次查看
jrdscl2006
Contributor I

I have a LPCXpresso LPC-Link 2 (LPC4370) that I am incorporating into a product. It would make my life easier if I could find a solid model (IGES) of the board or even drawings. Likely it is on the website somewhere, but I can not find it.

Help appreciated,

Joe

标签 (2)
0 项奖励
回复
2 回复数

1,650 次查看
jrdscl2006
Contributor I

@soledad Thanks! They don't have it either. I actually emailed them first....

Cheers,

Joe

0 项奖励
回复

1,650 次查看
soledad
NXP Employee
NXP Employee

Hi,

Please check more information about this board in the below link:

LPC-Link2 | Embedded Artists AB 


Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复