solid model LPC-Link 2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

solid model LPC-Link 2

1,737 Views
jrdscl2006
Contributor I

I have a LPCXpresso LPC-Link 2 (LPC4370) that I am incorporating into a product. It would make my life easier if I could find a solid model (IGES) of the board or even drawings. Likely it is on the website somewhere, but I can not find it.

Help appreciated,

Joe

Labels (2)
0 Kudos
Reply
2 Replies

1,654 Views
jrdscl2006
Contributor I

@soledad Thanks! They don't have it either. I actually emailed them first....

Cheers,

Joe

0 Kudos
Reply

1,654 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check more information about this board in the below link:

LPC-Link2 | Embedded Artists AB 


Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply