sdram initialization

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sdram initialization

1,957 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hamedb3269 on Sat Mar 07 09:06:12 MST 2015
This line is written for what purpose?
http://uupload.ir/files/pw5x_untitled.bmp
i am using K4S561632 or MT48LC16M16.
CLK Frequency is 120MHz.
CAS Latency is 3
RAS Latency is 3


Labels (1)
0 Kudos
Reply
1 Reply

1,913 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Sat Mar 07 10:58:41 MST 2015
Hi,
To configure SDRAM to a specific mode of operation. Command set the read latency, burst length,and burst type etc to be used during read/write operations to the SDRAM.
0 Kudos
Reply