sdram initialization

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sdram initialization

1,958件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hamedb3269 on Sat Mar 07 09:06:12 MST 2015
This line is written for what purpose?
http://uupload.ir/files/pw5x_untitled.bmp
i am using K4S561632 or MT48LC16M16.
CLK Frequency is 120MHz.
CAS Latency is 3
RAS Latency is 3


ラベル(1)
0 件の賞賛
返信
1 返信

1,914件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Sat Mar 07 10:58:41 MST 2015
Hi,
To configure SDRAM to a specific mode of operation. Command set the read latency, burst length,and burst type etc to be used during read/write operations to the SDRAM.
0 件の賞賛
返信