sd1 using SDK 2.10.1 dev_msc_disk_bm_SDIO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sd1 using SDK 2.10.1 dev_msc_disk_bm_SDIO

3,315件の閲覧回数
iblades_dan
Contributor II

Hello everyone,

I'm trying to bring up the dev_msc_disk_bm_SDIO example on my customer hardware with two SDMMC devices (MCU is LPC55S69 with one SDMMC device connected to SD0 and one SDMMC device connected to SD1).

If I use SD0 (g_sd.hostPort = 0), the card initializes properly, it enumerates to a PC and the PC can read/write SD0.

If I try the same for SD1 (g_sd.hostPort = 1), SD1 does not initialize successfully.  Instead the example code times out waiting for a kSD_Inserted event, even though there's a card in SD1.

Anyone have any insight into this issue?

 

Thanks,

DanL

ラベル(3)
0 件の賞賛
返信
4 返答(返信)

3,296件の閲覧回数
iblades_dan
Contributor II

Hi Alice, thanks for your quick reply!  Attached is a screenshot of the example I've imported.

Can you clarify what you mean by "other configuration?"

Best,

DanL

0 件の賞賛
返信

3,286件の閲覧回数
iblades_dan
Contributor II

Hi Alice, a quick update - I got SD1 working properly this evening.

Support for SD1 was only partially implemented in the example driver, an area I'd like to see NXP do better.

Implementing a driver function in "bits and pieces" often makes it harder to identify what's needed.

 

Regards,

DanL

0 件の賞賛
返信

3,254件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello DanL,

OK, thanks for your sharing and suggestion.

 

BR

Alice

0 件の賞賛
返信

3,306件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello iblades_dan,

How about other configuration?

And does the demo " dev_msc_disk_bm_SDIO "  under SDK? Is it the whole name? I haven't find this demo.

 

BR

Alice

 

0 件の賞賛
返信