sd1 using SDK 2.10.1 dev_msc_disk_bm_SDIO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sd1 using SDK 2.10.1 dev_msc_disk_bm_SDIO

5,010 Views
iblades_dan
Contributor II

Hello everyone,

I'm trying to bring up the dev_msc_disk_bm_SDIO example on my customer hardware with two SDMMC devices (MCU is LPC55S69 with one SDMMC device connected to SD0 and one SDMMC device connected to SD1).

If I use SD0 (g_sd.hostPort = 0), the card initializes properly, it enumerates to a PC and the PC can read/write SD0.

If I try the same for SD1 (g_sd.hostPort = 1), SD1 does not initialize successfully.  Instead the example code times out waiting for a kSD_Inserted event, even though there's a card in SD1.

Anyone have any insight into this issue?

 

Thanks,

DanL

Labels (3)
0 Kudos
Reply
4 Replies

4,991 Views
iblades_dan
Contributor II

Hi Alice, thanks for your quick reply!  Attached is a screenshot of the example I've imported.

Can you clarify what you mean by "other configuration?"

Best,

DanL

0 Kudos
Reply

4,981 Views
iblades_dan
Contributor II

Hi Alice, a quick update - I got SD1 working properly this evening.

Support for SD1 was only partially implemented in the example driver, an area I'd like to see NXP do better.

Implementing a driver function in "bits and pieces" often makes it harder to identify what's needed.

 

Regards,

DanL

0 Kudos
Reply

4,949 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello DanL,

OK, thanks for your sharing and suggestion.

 

BR

Alice

0 Kudos
Reply

5,001 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello iblades_dan,

How about other configuration?

And does the demo " dev_msc_disk_bm_SDIO "  under SDK? Is it the whole name? I haven't find this demo.

 

BR

Alice

 

0 Kudos
Reply