sct pwd with deadtime

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sct pwd with deadtime

1,342件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fusodeltutto on Sun Jul 21 09:35:52 MST 2013
Hi

I'm searching a code example to configure the SCT of an LPC810 to drive an Hbridge
in pwm for a dc motor.
I previously readed an NXP brochure at http://www.nxp.com/wcm_documents/techzones/microcontrollers-techzone/Presentations/dw2013-lpc800-pac...

where a SCT cookbook guide should contain, among others, a sct_pwm_deadtime code example.
I searched it in many places without find it ...
I also tried lpcopen platform but nothing
where I'm wrong ???

thank you all !
ラベル(1)
0 件の賞賛
返信
1 返信

1,319件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Fri Aug 09 11:39:07 MST 2013
There is a PWM with dead-time example in the SCT Cookbook and Tutorial which can be downloaded from:
http://www.lpcware.com/content/nxpfile/lpc80-sct-cookbook-and-tutorial-code-examples
0 件の賞賛
返信