running device and host mode at the same time for dual usb chip like lpc1850?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

running device and host mode at the same time for dual usb chip like lpc1850?

1,447件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cutemonster on Mon Apr 08 14:00:57 MST 2013

Hi, I saw the limitation note on the website and wonder if the usblib will support one USB device and one USB host for the lpc1850 chip.


The chip has 2 available USB ports.

ラベル(1)
  • USB

0 件の賞賛
返信
1 返信

1,438件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tuong on Mon Apr 08 23:32:11 MST 2013

Hi,


There is an example in LPCOpen running on LPC18xx, pls give it a try!


With best regards,

0 件の賞賛
返信