running device and host mode at the same time for dual usb chip like lpc1850?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

running device and host mode at the same time for dual usb chip like lpc1850?

1,442 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cutemonster on Mon Apr 08 14:00:57 MST 2013

Hi, I saw the limitation note on the website and wonder if the usblib will support one USB device and one USB host for the lpc1850 chip.


The chip has 2 available USB ports.

Labels (1)
0 Kudos
Reply
1 Reply

1,433 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tuong on Mon Apr 08 23:32:11 MST 2013

Hi,


There is an example in LPCOpen running on LPC18xx, pls give it a try!


With best regards,

0 Kudos
Reply