rs232 isp programmer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

rs232 isp programmer

4,792 Views
michaelcoffee
Contributor II

where can I find a stand alone

Tags (1)
5 Replies

4,208 Views
lpcxpresso_supp
NXP Employee
NXP Employee

If your board has an exposed debug circuit, you should go with a JTAG/SWD based flash programmer. As you say, there's several choices, and I suspect sufficiently portable. The salesperson has to connect a cable either way. Add a keyed socket on the board side to avoid trouble.

LPCXpresso Support

0 Kudos
Reply

4,209 Views
michaelcoffee
Contributor II

What I want is a unit which can be attached to the serial port of my board and used to program the processor.  This device would contain it's own processor and memory and operate independently not requiring a PC except to load the hex file to be programmed.

Yes I have Googled half the day with nothing to show for my effort.  There are any number of AVR devices but alas nothing I saw would work.

There are several stand-alone JTAG programmers but I need to put these in the hands of salesmen and I would expect problems.

4,209 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Please be more specific. Standalone can be interpreted. For example, if your board had a debug circuit, I would consider the LPCXpresso debug utility program standalone, since it can program flash independent of the LPCXpresso IDE. If you're looking for an unhosted solution, I'm not familiar with any. Such a programmer would at least require a serial port. A quick Google search revealed nothing which meets your requirements.

Thanks and regards,

LPCXpresso Support

0 Kudos
Reply

4,209 Views
michaelcoffee
Contributor II

This needs to be a stand-alone programmer.

0 Kudos
Reply

4,209 Views
lpcxpresso_supp
NXP Employee
NXP Employee
0 Kudos
Reply