"Free Running" DMA Mode on LPC55

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

"Free Running" DMA Mode on LPC55

ソリューションへジャンプ
2,176件の閲覧回数
rainyorange
Contributor I

Hi,

I'm currently working on a project that require DMA to be hardware triggered each time there is a rising edge generated by a clock on a GPIO pin.

For now I've managed to get the DMA working properly in "one shot mode" but I can't figure out how to configure the DMA to be triggered not once but each time there is a rising edge.

I think there in a bit to reset somewhere but I have no clue.

Here is the code :

volatile bool g_Transfer_Done = false;
dma_handle_t g_DMA_Handle;
static const int BUFF_LENGTH = 4U;
uint32_t dta = 0xAABBCCDD;

/* DMA descripter table used for ping-pong mode. */
SDK_ALIGN(uint32_t s_dma_table[2 * sizeof(dma_descriptor_t)], FSL_FEATURE_DMA_DESCRIPTOR_ALIGN_SIZE) = {0};

int cpt = 0;


void DMA_Callback(dma_handle_t *handle, void *param, bool transferDone, uint32_t tcds)
{
    if (transferDone)
    {
        cpt++;
    }
}
   
 
void DMA_Initialisation()
    {

        uint32_t xferConfig = DMA_CHANNEL_XFER(true,
                                               true,
                                               true,
                                              false,
                                                  4,
                      kDMA_AddressInterleave0xWidth,
                      kDMA_AddressInterleave1xWidth,
                                                  4
        );

        DMA_Init(DMA0);
        DMA_CreateHandle(&g_DMA_Handle, DMA0, 0);
        DMA_EnableChannel(DMA0, 0);
        DMA_SetCallback(&g_DMA_Handle, DMA_Callback, NULL);
        DMA_SetChannelConfig(DMA0, 0, &triggerConfig, false);
       
        PINT_Init(PINT);
        INPUTMUX_Init(INPUTMUX);
        INPUTMUX_AttachSignal(INPUTMUX, kPINT_PinInt0, kINPUTMUX_GpioPort1Pin28ToPintsel);
        INPUTMUX_AttachSignal(INPUTMUX, kPINT_PinInt0, kINPUTMUX_PinInt0ToDma0);
        INPUTMUX_Deinit(INPUTMUX); /* Turnoff clock to inputmux to save power. Clock is only needed to make changes */

        /* Clear Rise and Fall flags first */
        PINT->RISE = (1UL << kPINT_PinInt0);
        PINT->FALL = (1UL << kPINT_PinInt0);

        /* select level or edge sensitive */
        PINT->ISEL = (PINT->ISEL & ~(1UL << kPINT_PinInt0)) |
                    (((PINT_PIN_RISE_EDGE & PINT_PIN_INT_LEVEL) != 0U) ? (1UL << kPINT_PinInt0) : 0U);
           
        /* enable rising edge */    
        PINT->SIENR = 1UL << kPINT_PinInt0;

        //(void *)(&GPIO->PIN[1])
        DMA_PrepareChannelTransfer(&transferConfig,
                                              &dta,
                                    &destBuffer[0],
                                        xferConfig,
                               kDMA_MemoryToMemory,
                                    &triggerConfig,
             (dma_descriptor_t *)&(s_dma_table[0])
        );

        triggerConfig.type  = kDMA_RisingEdgeTrigger;
        triggerConfig.burst = kDMA_LevelBurstTransfer;
        triggerConfig.wrap  = kDMA_NoWrap;

        DMA_SubmitChannelTransfer(&g_DMA_Handle, &transferConfig);

        /* Set two DMA descripters to use ping-pong mode. */
        DMA_SetupDescriptor((dma_descriptor_t *)&(s_dma_table[0]), xferConfig, &dta,
                            (void *)destBuffer, (dma_descriptor_t *)&(s_dma_table[4]));
        DMA_SetupDescriptor((dma_descriptor_t *)&(s_dma_table[4]), xferConfig, &dta,
                            (void *)destBuffer, (dma_descriptor_t *)&(s_dma_table[0]));

        DMA_StartTransfer(&g_DMA_Handle);
    }
 
 
Note : I'm using a LPC55
 
Thank's for your attention 
ラベル(1)
0 件の賞賛
返信
1 解決策
2,158件の閲覧回数
rainyorange
Contributor I

Solution :

        NVIC_SetPriority(PIN_INT0_IRQn, 3);
        NVIC_ClearPendingIRQ(PIN_INT0_IRQn);
        EnableIRQ(PIN_INT0_IRQn);

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,159件の閲覧回数
rainyorange
Contributor I

Solution :

        NVIC_SetPriority(PIN_INT0_IRQn, 3);
        NVIC_ClearPendingIRQ(PIN_INT0_IRQn);
        EnableIRQ(PIN_INT0_IRQn);
0 件の賞賛
返信