"Deep Power Down" mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"Deep Power Down" mode

1,460 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by HammingBird on Sun May 29 08:25:39 MST 2016
Hallo,
I am using "LPC810". 

I would like to ask about   LPC810    "Deep Power Down" mode.  see more  in  user Manual --> 5.7.7

_______________________________________________________________________

5.7.7 Deep power-down mode:

During Deep power-down mode, the contents of the SRAM and registers are not retained
except for a small amount of data which can be stored in the general purpose registers of
the PMU block.
____________________________________________________________________

As I understood, in Deep power-down mode, once LPC810 enter in "Deep power-down mode" prog memory prog will be erased.

is it right ?

if so, then how LPC810  will work after wake up ? coz, prog has been erased ? 

Thanks 
Labels (1)
0 Kudos
Reply
2 Replies

1,268 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

1,268 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sun May 29 11:51:32 MST 2016

Quote: HammingBird
As I understood, in Deep power-down mode, once LPC810 enter in "Deep power-down mode" prog memory prog will be erased.

is it right ?



No, your program is usually in on-chip flash program memory  :O
0 Kudos
Reply