"15: Target error from Commit Flash Write" error when debugging the project on LPC55S69

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

"15: Target error from Commit Flash Write" error when debugging the project on LPC55S69

ソリューションへジャンプ
9,873件の閲覧回数
Emin
Contributor III

When I try to debug the project on LPC55S89, I got the Wire ACK Fault in DAP access within the error from the title. I also had to combine 2 rams in order to have enough space for the project. Can someone suggest their already working solution?

0 件の賞賛
返信
1 解決策
9,829件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Emin 

You can allocate some data to other RAM, detail method refer to:

<MCUXpresso IDE User Guider> ->
"18.13.2 Placing data into different RAM blocks using Macros"

I also attach it for you.

 

BR

Alice

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
9,845件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Emin 

It seems can not combine 2 rams, allocate it to different RAMS.

About the debug failed, how about debugging simple demo under SDK?

 

BR

Alice

0 件の賞賛
返信
9,837件の閲覧回数
Emin
Contributor III

How can I allocate the 271KB over 2 SRAMS without combining them? or how can I distribute 271KB over multiple SRAMs?

0 件の賞賛
返信
9,830件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Emin 

You can allocate some data to other RAM, detail method refer to:

<MCUXpresso IDE User Guider> ->
"18.13.2 Placing data into different RAM blocks using Macros"

I also attach it for you.

 

BR

Alice

0 件の賞賛
返信