questions about CAN controller acceptance filter in LPC2000

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

questions about CAN controller acceptance filter in LPC2000

1,622件の閲覧回数
jacktan
Contributor I

Hi expert,

I would like to use CAN controller acceptance filter to mask out the IDs that I don't want to receive, can you please help me share the demo source code with me?

That would be perfect if you have some documents to describe this feature more detailed than the user manual?

Regards,

Jack 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,451件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Jack,

You could refer to the following links, which provides useful information regarding acceptance filters:

https://developer.mbed.org/forum/mbed/topic/2033/

http://www.keil.com/forum/14320/lpc2129-can-register-initialization/

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信