on power on LPC1769, the code isn't executed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

on power on LPC1769, the code isn't executed

5,104 Views
pedromoreira
Contributor I

Hi all, i'm testing LPC1769 on a LPCxpresso board, when I use debugger on IDE, the code is executed OK but when I power UP the board the code isn't executed, what is wrong?

many thanks

pmoreira

0 Kudos
Reply
6 Replies

4,893 Views
pedromoreira
Contributor I

Hi, the original problem was produced  for a "printf()"  statement, deleting this instruction the problem don't occur. I think that the cause for this anomaly is that the debug module load  automatically the library that contain the code for the printf statement.

thanks

pmoreira

0 Kudos
Reply

4,893 Views
ronwal
Contributor III

Hi, I´ve got the same problem. What is the cause for that?

On OM13000 it worked before.

My project is based on the uIP/ webserver sample.

br

Ron

0 Kudos
Reply

4,891 Views
brendonslade
NXP TechSupport
NXP TechSupport

This can be caused by an external reset being applied to the LPC11U35 debug probe on the board as the board starts up. The attached notes from Embedded Artists explain the problem and how to modify the board to avoid it.

0 Kudos
Reply

4,891 Views
ronwal
Contributor III

I´m using the OM13085 eval. board and it seems to behave differently than the OM13000, which I used before.

Where can I find the information exactly?

Thanks

Ron

0 Kudos
Reply

4,891 Views
brendonslade
NXP TechSupport
NXP TechSupport

Its an attachment to my response above (the LPCXpresso1769 CD Rev D Product Note PDF file.)

0 Kudos
Reply

4,891 Views
brendonslade
NXP TechSupport
NXP TechSupport

What code are you running and on which board exactly (OM13085?)

Did you try this using periph_blinky from the LPCOpen package?

0 Kudos
Reply