nxpUSBlib support area? ...and if so, library configuration question.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

nxpUSBlib support area? ...and if so, library configuration question.

1,074件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sjalloq on Tue Nov 08 15:56:46 MST 2011
Just wanted to check if this is the correct forum to ask questions regarding the usage of nxpUSBlib with the lpcxpresso IDE?

If it is, then I'd like to point out a bug/feature in the Linux IDE.  You configuration instructions tell you to, "Click Project->Build Configurations->Set Active-> and select the...".  However, this doesn't result in any sort of pop up window or selection box appearing.  If I instead right click on the project in question and navigate to "Build Configurations ->Set Active..." then I can select the relevant option.

I'm running v4.1.0 [build 164] on Ubuntu 11.04.

Shareef.
ラベル(1)
  • USB

0 件の賞賛
返信
1 返信

1,061件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxpUSBlib team on Tue Nov 08 18:27:36 MST 2011
Thanks for pointing this out. We have not done any testing on Linux yet so this is useful information. We will be changing that section of the Build It page to make it more clear and I will switch over to using the 'right-click on the project in question' method since that works in the Windows version too.
0 件の賞賛
返信