nxpUSBLib/libraries/CDL/LPC17xxLib should include IAP code from AN11071

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

nxpUSBLib/libraries/CDL/LPC17xxLib should include IAP code from AN11071

1,497 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by triffid_hunter on Tue Jul 03 09:28:26 MST 2012
hi,

nxpUSBLib includes IAP code for lpc17[78]x but not lpc17[56]x even though code for lpc17[56]x is available from AN11071

I believe that nxpUSBLib should include the code from AN11071.

Maybe even update it every so often, such as renaming 'void u32IAP_ReadSerialNumber' to 'void vIAP_ReadSerialNumber' for consistency, or putting in the actual description for u32IAP_ReadSerialNumber instead of having identical information as the quite different u32IAP_ReadBootVersion ;)
标签 (1)
0 项奖励
回复
1 回复

1,470 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tuong on Wed Jul 04 18:56:14 MST 2012
Dear triffid_hunter,

I see that the chip's drivers inside nxpUSBlib is nearly same as the one that NXP release for their seperate chips driver, so this issue may caused by nxpUSBlib LPC175x_6x chip driver is not updated?! But I think this is not a big deal, you can make it your self for your own need!

With best regards!
0 项奖励
回复