no emulator or board available. this could be because it is unpowered unconnected or already in use

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

no emulator or board available. this could be because it is unpowered unconnected or already in use

1,219件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pdrodriguez on Fri Oct 05 10:48:05 MST 2012
I just tried to program the lpc 1769 and tells me


"No emulator or board available. This Could Be Because It is unpowered unconnected or already in use"


I did nothing, 1 week ago on uC leave it with a program that worked and I was changing the routines to analyze response times with counters and never shot any error, and now will not let me schedule and stick with the program I leave last week.

Try connecting the uC with pin P2 [10] grounded but still let me programmed.

Anyone know what I can do?
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,209件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Daniel Widyanto on Mon Oct 08 21:25:29 MST 2012
Hi,

The message usually comes out if the MCU is not powered. Check your board's connection and power supply, make sure that the 3.3V VCC is there.

0 件の賞賛
返信

1,209件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pdrodriguez on Fri Oct 05 10:51:18 MST 2012
Also change the USB cable to connect it to the pc, but still doing the same.
0 件の賞賛
返信