need lpc824 uart codings

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

need lpc824 uart codings

3,169 次查看
aravindpb5009
Contributor III

hai 

please share me basic uart coding for lpc824 

thanks and regards 

aravind p

标签 (1)
0 项奖励
回复
7 回复数

3,094 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Aravind palanisamy 

LPC824 ADC basic demo is included in SDK package. here is to build and download SDK for LPC824

Welcome | MCUXpresso SDK Builder 

"lpc_adc_basic" demo location path:

{SDK_package install folder}\boards\lpcxpresso824max\driver_examples\adc


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

3,094 次查看
aravindpb5009
Contributor III

thank you

0 项奖励
回复

3,094 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Welcome!

0 项奖励
回复

3,094 次查看
aravindpb5009
Contributor III

i need some uart basic codings plz  share me

0 项奖励
回复

3,094 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

You can find uart demo code in SDK package too:

{SDK_package install folder}\boards\lpcxpresso824max\driver_examples\usart

under this folder there are 6 uart demo code. in each demo code folder there is readme.txt, please read them to see which one match your requirement.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

3,094 次查看
aravindpb5009
Contributor III

Thank you...................................................................

0 项奖励
回复

3,094 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

you are welcome.

0 项奖励
回复