need bootloader files for LPC1549JBD64 and LPC1549JBD48

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

need bootloader files for LPC1549JBD64 and LPC1549JBD48

1,153 Views
gipis33422
Contributor I

i am complete beginner to microcontroller can you please tell me that which software do i use to upload boot loader to LPC1549JBD64 and which programmer should i use. Can stlink v2 will work or not please give me bootloader file for LPC1549JBD64 and LPC1549JBD48

0 Kudos
Reply
1 Reply

1,099 Views
soledad
NXP Employee
NXP Employee

Hi,

You can use LPC link-2. Firmware can easily be loaded into the board using the free LPCScrypt utility, which runs on Windows (7/8/10), MacOS and Linux. Note that when using LPCXpresso IDE or MCUXpresso IDE, no firmware programming is required.

I suggest using MCUXpresso IDE and LPCOpen drivers.

You can download MCUXpresso IDE and LPCOpen from the following links:

MCUXpresso IDE|Eclipse-based Integrated Development Environment (IDE) | NXP 

LPCOpen Libraries and Examples | NXP 

Regards

Soledad

0 Kudos
Reply