multicore project using SPIFI flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

multicore project using SPIFI flash

1,664 Views
smarty760
Contributor I

Hi, 

I am trying to create a multicore project using SPIFI flash and I have a few questions about this. The processor I am using is LPC4370 with lpc link 2. I am trying to do what is seen at the end of this post: https://community.nxp.com/t5/LPC-Microcontrollers/MULTICORE-M4-M0App-Memory-Map-Issues-at-compile-ti....

This is putting the M0 project into the second flash part and second RAM part, while the M4 project stays in the first flash part and first RAM part. In the post, I saw that the LPC18_43_SPFI_16MB_64KB.cfx flash driver is used. Does this still have to be used? Where can I download this? I replaced this with the LPC_43_SPFI_GENERIC.cfx. I am not sure If I am supposed to do this.

I created a M0 and M4 project to do this. The m4 project starts fine but I get an error when the M0 app needs to start.

Error:

smarty760_0-1687334716159.png

 

 

M4 project memory:

smarty760_1-1687334716183.png

 

 

M0 project memory:

smarty760_2-1687334716193.png

 

 

Labels (3)
0 Kudos
Reply
1 Reply

1,579 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @smarty760 

 

I attach it for you.

 

BR

Alice

 

0 Kudos
Reply