mbed driver size issue on PC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mbed driver size issue on PC

1,487件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by yingweib on Tue May 20 02:32:50 MST 2014
Hi,

As 1549 does not have external flash(LPC1768 had 2MB external flash) and only had on-chip flash, which should be 256KB from the data sheet, why it showed 512KB in the driver on PC? does 1549 have external flash as well?

Can someone help to clarify this? thanks a lot.

Daniel

ラベル(1)
0 件の賞賛
返信
1 返信

1,471件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue May 20 07:45:16 MST 2014
Yes, LPC1549 has a 256KB of internal flash.

I believe that this incorrect report from the mbed flash device will be fixed in a forthcoming update of the LPCXpresso1549 mbed firmware.

Regards,
LPCXpresso Support
0 件の賞賛
返信