maximum output timer lpc4337

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

maximum output timer lpc4337

1,355件の閲覧回数
diegotorres
Contributor I

hi I'm working on lpc4337 and I'm trying generate an output with a timer as 10mhz frequency and I just can get approximately 300khz. That's possible?get an output higher as 10mhz??regards

タグ(1)
0 件の賞賛
返信
1 返信

1,216件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Which timer are you using?

Please check the AN11538 application note, this application note is a collection of examples and usage notes for the
SCTimer/PWM block used in NXP microcontrollers.

http://www.nxp.com/documents/application_note/AN11538.zip 

I hope this helps,

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信