lwIP - timeouts and re-init

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lwIP - timeouts and re-init

2,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tamirmichael on Wed Sep 26 05:32:25 MST 2012
Hello,

I use lwIP in one commercial product (LPC2478) and intend to continue to use it in a future LPC1788-based product as well.
I am wondering how I can best deal with traffic being disturbed by pulling out the network cable - yes, this event can be detected by lwIP, but the port uses several FreeRTOS synchronization resources (semaphores...) that might be locked/held by the time, for example, a new IP address is needed (consider for example one pulling out the cable while data is transferred, followed by disabling DHCP and then enabling DHCP). I tried to kill these resources but I did not manage to get it right yet.
I was wondering what the appropriate way to restart the lwIP port actually is (in case, for example, a transfer timeout is detected) ?

Thanks in advance
Labels (1)
0 Kudos
Reply
1 Reply

1,903 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Daniel Widyanto on Thu Sep 27 00:44:51 MST 2012
Hi,

Just suggestion, I think you'll have more luck asking this question to lwIP mailing list (http://savannah.nongnu.org/mail/?group=lwip)

Regards,
-daniel
0 Kudos
Reply