lpx43xx usb0 host HID keyboard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpx43xx usb0 host HID keyboard

1,959 Views
shivrajtbm
Contributor I

HI 

i'm using lpx4357 and successfully completed keyboard interfacing using USB HID but when i connect a barcode scanner hard fault occurs after scanning .. only one byte read / detected and then it goes to hard fault.. can i get some ideas why this could be happen?? or any suggestions ?

 

please help!

Labels (3)
0 Kudos
Reply
3 Replies

1,951 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Is your project based on lpcopen demo ? if yes which one? any revise ?

Please track where runs to error? Does it enumerate well?

0 Kudos
Reply

1,935 Views
shivrajtbm
Contributor I

issue solved .. thank you..

0 Kudos
Reply

1,256 Views
Md_Rdgc
Contributor I

Hi,

I am trying to interface the USB barcode scanner. I am using the LPCOpen Keyboard Host example, I am getting the keyboard keys. But when I connect the barcode scanner, it shows device is enumerated, but now able to read the barcode data. Can you please let me know, what modification need to be done in the keyboard code example to read the barcode data. 

Controller LPC4337

Barcode Make Newland.

Model NLS-HR11

Warm regards.

 

0 Kudos
Reply