lpcxpresso824-max

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpcxpresso824-max

836件の閲覧回数
Daniel_Robinson
Contributor I

I got a lpcxpresso824-max, version 2.  I note that it has a JP3 on it, and it seems that the documents on line do not include this.  At nxp.com, the schematics and docs are for version 1 and need to be updated.

On my Windows 11 machine, the board showed up only as a drive, USB MSC.  This was also true when I plugged it into my Linux machine.

There were no directions or firmware that I could find for the LPC11U35 on nxp.com, but I found instructions on os.mbed.com, https://os.mbed.com/platforms/LPCXpresso824-MAX/ and updated the firmware using a Windows10 machine at home.  The board now shows up as a drive and USB_CDC on my Linux machine and I was able to use the LPC11U35 to program and debug the board, but still does not appear on my Windows11 machine.

This is the output of lsusb -v from my Linux machine.

Bus 001 Device 015: ID 0d28:0204 NXP ARM mbed
Device Descriptor:
bLength 18
bDescriptorType 1
bcdUSB 1.10
bDeviceClass 2 Communications
bDeviceSubClass 0
bDeviceProtocol 0
bMaxPacketSize0 8
idVendor 0x0d28 NXP
idProduct 0x0204 ARM mbed
bcdDevice 1.00
iManufacturer 1 MBED
iProduct 2 MBED CMSIS-DAP
iSerial 3 0824022111466540EC98929C
bNumConfigurations 1
Configuration Descriptor:
bLength 9
bDescriptorType 2
wTotalLength 0x007a
bNumInterfaces 4
bConfigurationValue 1
iConfiguration 0
bmAttributes 0x80
(Bus Powered)
MaxPower 500mA
Interface Descriptor:
bLength 9
bDescriptorType 4
bInterfaceNumber 0
bAlternateSetting 0
bNumEndpoints 2
bInterfaceClass 8 Mass Storage
bInterfaceSubClass 6 SCSI
bInterfaceProtocol 80 Bulk-Only
iInterface 7 USB_MSC
Endpoint Descriptor:
bLength 7
bDescriptorType 5
bEndpointAddress 0x82 EP 2 IN
bmAttributes 2
Transfer Type Bulk
Synch Type None
Usage Type Data
wMaxPacketSize 0x0040 1x 64 bytes
bInterval 0
Endpoint Descriptor:
bLength 7
bDescriptorType 5
bEndpointAddress 0x02 EP 2 OUT
bmAttributes 2
Transfer Type Bulk
Synch Type None
Usage Type Data
wMaxPacketSize 0x0040 1x 64 bytes
bInterval 0
Interface Descriptor:
bLength 9
bDescriptorType 4
bInterfaceNumber 1
bAlternateSetting 0
bNumEndpoints 1
bInterfaceClass 2 Communications
bInterfaceSubClass 2 Abstract (modem)
bInterfaceProtocol 1 AT-commands (v.25ter)
iInterface 4 USB_CDC
CDC Header:
bcdCDC 1.10
CDC Call Management:
bmCapabilities 0x03
call management
use DataInterface
bDataInterface 2
CDC ACM:
bmCapabilities 0x06
sends break
line coding and serial state
CDC Union:
bMasterInterface 1
bSlaveInterface 2
Endpoint Descriptor:
bLength 7
bDescriptorType 5
bEndpointAddress 0x83 EP 3 IN
bmAttributes 3
Transfer Type Interrupt
Synch Type None
Usage Type Data
wMaxPacketSize 0x0010 1x 16 bytes
bInterval 32
Interface Descriptor:
bLength 9
bDescriptorType 4
bInterfaceNumber 2
bAlternateSetting 0
bNumEndpoints 2
bInterfaceClass 10 CDC Data
bInterfaceSubClass 0
bInterfaceProtocol 0
iInterface 5 USB_CDC1
Endpoint Descriptor:
bLength 7
bDescriptorType 5
bEndpointAddress 0x04 EP 4 OUT
bmAttributes 2
Transfer Type Bulk
Synch Type None
Usage Type Data
wMaxPacketSize 0x0040 1x 64 bytes
bInterval 0
Endpoint Descriptor:
bLength 7
bDescriptorType 5
bEndpointAddress 0x84 EP 4 IN
bmAttributes 2
Transfer Type Bulk
Synch Type None
Usage Type Data
wMaxPacketSize 0x0040 1x 64 bytes
bInterval 0
Interface Descriptor:
bLength 9
bDescriptorType 4
bInterfaceNumber 3
bAlternateSetting 0
bNumEndpoints 2
bInterfaceClass 3 Human Interface Device
bInterfaceSubClass 0
bInterfaceProtocol 0
iInterface 6 MBED CMSIS-DAP
HID Device Descriptor:
bLength 9
bDescriptorType 33
bcdHID 1.00
bCountryCode 0 Not supported
bNumDescriptors 1
bDescriptorType 34 Report
wDescriptorLength 33
Report Descriptors:
** UNAVAILABLE **
Endpoint Descriptor:
bLength 7
bDescriptorType 5
bEndpointAddress 0x81 EP 1 IN
bmAttributes 3
Transfer Type Interrupt
Synch Type None
Usage Type Data
wMaxPacketSize 0x0040 1x 64 bytes
bInterval 1
Endpoint Descriptor:
bLength 7
bDescriptorType 5
bEndpointAddress 0x01 EP 1 OUT
bmAttributes 3
Transfer Type Interrupt
Synch Type None
Usage Type Data
wMaxPacketSize 0x0040 1x 64 bytes
bInterval 1
Device Status: 0x0000
(Bus Powered)

0 件の賞賛
返信
0 返答(返信)