lpcxpresso55s16_freertos_spi example can not find in SDK v2.14.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpcxpresso55s16_freertos_spi example can not find in SDK v2.14.0

Jump to solution
1,918 Views
felix1
Contributor IV

Hi,

I can find a freertos SPI example in LPC55S16 SDK v2.13.0, but I can not find it in SDK v2.14.0. The freertos SPI example is indeed remove from SDK v2.14.0 or I miss something in SDK builder?

Labels (1)
0 Kudos
Reply
1 Solution
1,890 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Yes, the version 2.14.0 of SDK package for LPC55S16 has removed the freertos_spi,freertos_usart, and freertos_i2c examples, I have downloaded the package, I copy the directory.

BR

XiangJun Rong

 

xiangjun_rong_0-1691029516270.png

 

View solution in original post

0 Kudos
Reply
5 Replies
1,909 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Can you tell us the lpcxpresso55s16_freertos_spi example directory in the old version LPC55S16 SDK v2.13.0?

BR

XiangJun Rong

0 Kudos
Reply
1,904 Views
felix1
Contributor IV

Hi,

The directory is \SDK_2_13_0_LPCXpresso55S16\boards\lpcxpresso55s16\rtos_examples\freertos_spi

 

0 Kudos
Reply
1,891 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Yes, the version 2.14.0 of SDK package for LPC55S16 has removed the freertos_spi,freertos_usart, and freertos_i2c examples, I have downloaded the package, I copy the directory.

BR

XiangJun Rong

 

xiangjun_rong_0-1691029516270.png

 

0 Kudos
Reply
1,850 Views
felix1
Contributor IV

Hi,

Why NXP removed the freertos_spi example from SDK v2.14.0?

Because I use freertos_spi example as my project's code base, I need to know if there is any bug in this example.

0 Kudos
Reply
1,815 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

You can use the old version of lpcxpresso55s16_freertos_spi example, there is not bug for the example.

BR

XiangJun Rong

0 Kudos
Reply