lpcxpresso55s16_freertos_spi example can not find in SDK v2.14.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpcxpresso55s16_freertos_spi example can not find in SDK v2.14.0

ソリューションへジャンプ
1,995件の閲覧回数
felix1
Contributor IV

Hi,

I can find a freertos SPI example in LPC55S16 SDK v2.13.0, but I can not find it in SDK v2.14.0. The freertos SPI example is indeed remove from SDK v2.14.0 or I miss something in SDK builder?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,967件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Yes, the version 2.14.0 of SDK package for LPC55S16 has removed the freertos_spi,freertos_usart, and freertos_i2c examples, I have downloaded the package, I copy the directory.

BR

XiangJun Rong

 

xiangjun_rong_0-1691029516270.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
1,986件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Can you tell us the lpcxpresso55s16_freertos_spi example directory in the old version LPC55S16 SDK v2.13.0?

BR

XiangJun Rong

0 件の賞賛
返信
1,981件の閲覧回数
felix1
Contributor IV

Hi,

The directory is \SDK_2_13_0_LPCXpresso55S16\boards\lpcxpresso55s16\rtos_examples\freertos_spi

 

0 件の賞賛
返信
1,968件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Yes, the version 2.14.0 of SDK package for LPC55S16 has removed the freertos_spi,freertos_usart, and freertos_i2c examples, I have downloaded the package, I copy the directory.

BR

XiangJun Rong

 

xiangjun_rong_0-1691029516270.png

 

0 件の賞賛
返信
1,927件の閲覧回数
felix1
Contributor IV

Hi,

Why NXP removed the freertos_spi example from SDK v2.14.0?

Because I use freertos_spi example as my project's code base, I need to know if there is any bug in this example.

0 件の賞賛
返信
1,892件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

You can use the old version of lpcxpresso55s16_freertos_spi example, there is not bug for the example.

BR

XiangJun Rong

0 件の賞賛
返信