lpcopen periphiral code for lpc17xx.. does not compile under Linux.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpcopen periphiral code for lpc17xx.. does not compile under Linux.

1,359件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Tue Jun 11 12:21:34 MST 2013

  Dear list,


 lpcxpresso v5.2.4 does not compile (probably) all periph-projects from  lpcopen v1.03.


The nxp_xpresso_1769_board_lib library compiles fine.


The reason is that the include and library pathnames in these projects contain "\" as the path separator,  not "/".


After changing all separators it works fine.


I don't know whether this is the proper solution with respect to windows.


    Regards,


        Sietse

ラベル(1)
0 件の賞賛
返信
0 返答(返信)