lpc54616 can bus error managment

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

lpc54616 can bus error managment

3,409 次查看
ali3
Contributor II

How can dedect bus off state an other can bus error im lpc 54616? im try in mcan interrupt transfer like this:

case kStatus_MCAN_ErrorStatus:
{
uint32_t bo, lec;

if ((base->PSR&CAN_PSR_BO_MASK)>>CAN_PSR_BO_SHIFT)
{

/* Reset INIT bit to enter normal mode. */
base->CCCR &= ~CAN_CCCR_INIT_MASK;
while (0U != (base->CCCR & CAN_CCCR_INIT_MASK))
{
}

while ( (((base->PSR&CAN_PSR_LEC_MASK)==5) ) || (((base->PSR&CAN_PSR_BO_MASK)>>CAN_PSR_BO_SHIFT==1)) )
{

}


MCAN_Init(EXAMPLE_MCAN, &mcanConfig, MCAN_CLK_FREQ);
//MCAN_Deinit(base);
}


//MCAN_Init(EXAMPLE_MCAN, &mcanConfig, MCAN_CLK_FREQ);
//MCAN_Deinit(base);//Init(EXAMPLE_MCAN, &mcanConfig, MCAN_CLK_FREQ);


}

But PSR_BO always is 1

标签 (1)
0 项奖励
回复
5 回复数

3,324 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Ali,

I see that you just want to handle various error.

You can manipulate the NCAN0_RST in PRESETCTRL1 REG to reset the CAN module, then reinitialize the CAN module.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

0 项奖励
回复

3,324 次查看
ali3
Contributor II

i can solve this problem . I can grab error in calback function. after ican restart can modul with bus_off.  But important function sendnonblocking method. if user use like sdk is hangup in while statement

while (!txComplete)
{

}
txComplete = false;

user must control sendnonblocikng methode return value. If valu is sucsec u can use while statement.

sts=MCAN_TransferSendNonBlocking(EXAMPLE_MCAN, &mcanHandle, &txXfer);


switch (sts)
{

case kStatus_Success:
{
while (!txComplete)
{

}
txComplete = false;

}
break;

case kStatus_Fail:
{
psr=EXAMPLE_MCAN->PSR&CAN_PSR_LEC_MASK;
ecer=EXAMPLE_MCAN->ECR&CAN_ECR_TEC_MASK;
busof=(EXAMPLE_MCAN->PSR&CAN_PSR_BO_MASK)>>CAN_PSR_BO_SHIFT;
ccr=EXAMPLE_MCAN->CCCR;
sts=0;

}

break;
case kStatus_MCAN_TxBusy:
{


}

default:
break;

}

call back func:

static void mcan_callback(CAN_Type *base, mcan_handle_t *handle, status_t status, uint32_t result, void *userData)
{
BaseType_t xHigherPriorityTaskWoken;

/* The xHigherPriorityTaskWoken parameter must be initialized to pdFALSE as
it will get set to pdTRUE inside the interrupt safe API function if a
context switch is required. */
xHigherPriorityTaskWoken = pdFALSE;

/* 'Give' the semaphore to unblock the task. */


/* Pass the xHigherPriorityTaskWoken value into portYIELD_FROM_ISR(). If
xHigherPriorityTaskWoken was set to pdTRUE inside xSemaphoreGiveFromISR()
then calling portYIELD_FROM_ISR() will request a context switch. If
xHigherPriorityTaskWoken is still pdFALSE then calling
portYIELD_FROM_ISR() will have no effect. The implementation of
portYIELD_FROM_ISR() used by the Windows port includes a return statement,
which is why this function does not explicitly return a value. */

// printf("Callback status: 0x%x", status);
//printf(" IR: 0x%x \r\n", base->IR);


switch (status)
{


case kStatus_MCAN_RxFifo0Idle:
{

xSemaphoreGiveFromISR( semaphoreRX, &xHigherPriorityTaskWoken );
rxComplete = true;
portYIELD_FROM_ISR( xHigherPriorityTaskWoken );
}
break;

case kStatus_MCAN_TxIdle:
{
xSemaphoreGiveFromISR( semaphorum, &xHigherPriorityTaskWoken );
txComplete = true;
portYIELD_FROM_ISR( xHigherPriorityTaskWoken );
}
break;

case kStatus_MCAN_ErrorStatus:
{
if (EXAMPLE_MCAN->CCCR &= CAN_CCCR_INIT_MASK)
{
EXAMPLE_MCAN->CCCR &= ~CAN_CCCR_INIT_MASK;
while (0U != (EXAMPLE_MCAN->CCCR & CAN_CCCR_INIT_MASK))
{
}
}


mcanreset();
//txError=true;
txComplete = true;
xSemaphoreGiveFromISR( semaphorum, &xHigherPriorityTaskWoken );
txComplete = true;
portYIELD_FROM_ISR( xHigherPriorityTaskWoken );


}

default:
break;
}
}

in calback function i send xsemaphore to my rtos but this is only evaluate .

sory this code only evaluate. im writing all is next day. 

0 项奖励
回复

3,324 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Ali,

For the CAN bus off error, pls check the CAN bus network, the CANx_TD and CANx_RD must be connected to a CAN transceiver, as Frank said that the 120 ohm terminating resistor between CAN_H and CAN_L pins of CAN transceiver is required.

BR

XiangJun Rong

0 项奖励
回复

3,324 次查看
ali3
Contributor II

My can cominication work.İ neede manupilating can buss error state. I can try in sdk example . Can work normal but if i can short circuit can bus can  goes bus off state .  How can i reset cominication and other error state. 

0 项奖励
回复

3,324 次查看
frank_m
Senior Contributor III

Check the error counter values (TEC and REC).

These values are implemented according to the CAN bus standard.

"Bus off" means a counter (usually TEC) has hit 255.

It seems you have a physical problem, perhaps your termination is not correct, or you swapped CANH and CANL at one bus participant.

0 项奖励
回复