lpc54606

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc54606

1,588件の閲覧回数
344144584
Contributor I

Using the LPC54606 chip to do the game, I found that it was normal at the beginning, but after some time of power-on, the pulse voltage of some pins of the chip is abnormal. After power-off, it will return to normal after power-on again. This kind of problem often occurs, what will be? Caused by?

ラベル(1)
0 件の賞賛
返信
1 返信

1,394件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

Could you share the schematic file?


Have a great day,
Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信