lpc54414 adc reading not getting api code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc54414 adc reading not getting api code

1,177 Views
santoshganachar
Contributor II

adc value is not getting .

0 Kudos
Reply
1 Reply

1,126 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

Please refer to the following link:

Download the corresponding LPCOpen depending on the IDE that you are currently using. In the LPCOpen package you will find a example of the adc (periph_adc). You can use this as a guide to your project.

Also, I highly recommend you to read the user manual: UM10914.pdf   chapter 29 that corresponds to the adc. 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply