lpc541xx PLL Calculator

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

lpc541xx PLL Calculator

跳至解决方案
1,983 次查看
hk123
Contributor I

Hello All,

I am wondering if there is a reference utility pll calculator I can use.

Basically I have a board which has 25Mhz external crystal and I want to have the system clock to be 96 Mhz.

Can some one guide me as to PLL register settings I can use.

 

Best Regards.

0 项奖励
回复
1 解答
1,972 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

I'd recommend to use the clock config tool. Here you have a user friendly diagram which will help you configure the PLL accordingly. It also provides warnings when exceeding the limits of multiplier and divider. I attempted to get a 96 MHz system clock from 25 MHz input and got close but not exactly.

nxf51209_0-1599888291894.png

For more details on how to use the clock config tool, please review the Config Tool user guide.

Best Regards,

Sabina

在原帖中查看解决方案

3 回复数
1,973 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

I'd recommend to use the clock config tool. Here you have a user friendly diagram which will help you configure the PLL accordingly. It also provides warnings when exceeding the limits of multiplier and divider. I attempted to get a 96 MHz system clock from 25 MHz input and got close but not exactly.

nxf51209_0-1599888291894.png

For more details on how to use the clock config tool, please review the Config Tool user guide.

Best Regards,

Sabina

1,958 次查看
hk123
Contributor I

This is perfect. Thanks Sabina.

0 项奖励
回复
1,943 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Glad to help!

0 项奖励
回复