lpc541xx PLL Calculator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc541xx PLL Calculator

ソリューションへジャンプ
2,888件の閲覧回数
hk123
Contributor I

Hello All,

I am wondering if there is a reference utility pll calculator I can use.

Basically I have a board which has 25Mhz external crystal and I want to have the system clock to be 96 Mhz.

Can some one guide me as to PLL register settings I can use.

 

Best Regards.

0 件の賞賛
返信
1 解決策
2,877件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

I'd recommend to use the clock config tool. Here you have a user friendly diagram which will help you configure the PLL accordingly. It also provides warnings when exceeding the limits of multiplier and divider. I attempted to get a 96 MHz system clock from 25 MHz input and got close but not exactly.

nxf51209_0-1599888291894.pngnxf51209_0-1599888291894.png

For more details on how to use the clock config tool, please review the Config Tool user guide.

Best Regards,

Sabina

元の投稿で解決策を見る

3 返答(返信)
2,878件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

I'd recommend to use the clock config tool. Here you have a user friendly diagram which will help you configure the PLL accordingly. It also provides warnings when exceeding the limits of multiplier and divider. I attempted to get a 96 MHz system clock from 25 MHz input and got close but not exactly.

nxf51209_0-1599888291894.pngnxf51209_0-1599888291894.png

For more details on how to use the clock config tool, please review the Config Tool user guide.

Best Regards,

Sabina

2,863件の閲覧回数
hk123
Contributor I

This is perfect. Thanks Sabina.

0 件の賞賛
返信
2,848件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Glad to help!

0 件の賞賛
返信