lpc54114 no PwmOut in mbed OS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc54114 no PwmOut in mbed OS

1,898 Views
NBur
Contributor I

Hi,

The LPC 54114 has no mbed class for PwmOut making it impossible to use PWM directly in mbed OS although its advertised as available.

 

Any way to go around this?

The issue seems to exist at least since 2018.

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,892 Views
converse
Senior Contributor V

This is probably better addressed on the mBed OS support forum:

https://forums.mbed.com/c/mbed-os/6

0 Kudos
Reply

1,884 Views
NBur
Contributor I

Thanks for the reply

 

I have asked in mbed forums but had no help there.

It was suggested to me that the wrapping of the SDK to the Mbed API is actually done by NXP thus the question on this forum.

0 Kudos
Reply